Add an HMI Device
To control your application,
It can also be embedded into targeted Controllers.
- Modbus TCP Tool Center Point - The point in the machine that is commanded to move, typically the center or the head of the tool. It can be described in different coordinate systems. is used for communication from an HMI panel's Ethernet Ethernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs). port to the X32 connector on the top of a AKD PDMM or PCMM.
- Modbus Modbus® is a serial communications protocol. it is the most commonly available means of connecting industrial electronic devices. Modbus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the Modbus protocol exist for serial port and Ethernet. It is widely used with TCP/IP over Ethernet. communication may be active while programming The act of performing a sequence of instructions or commands. the controller through the KAS-IDE Kollmorgen Automation Suite - Integrated Development Environment while the AKD PDMM or PCMM is connected to a network, switch, or hub.
- The KAS Kollmorgen Automation Suite-IDE Integrated Development Environment - An type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. is automatically linked to the KVB Kollmorgen Visual Builder for HMI HMI development software, and the Modbus addresses are automatically set.
- See KDN for more information.
When running the KAS Simulator, an internal HMI editor is also available to debug the application.
See Design the HMI with the Internal Editor for more information.